![]() |
Accelerate your next IoT node design with the BlueNRG-Tile, a 1-inch coin-shaped Bluetooth multi-sensor module development kit |
Watch and learn how to simplify the integration of sensors, a Bluetooth Low Energy system-on-chip (SoC), and sensor fusion libraries into your next IoT design using the BlueNRG-Tile development kit (STEVAL-BCN002V1B).
This tiny device consists of a 1-inch diameter coin-shaped board containing a low power inertial module (accelerometer + gyroscope), state-of-the-art magnetometer, a Time-of-Flight proximity sensor with a 4 m detection capability, pressure sensor, humidity and temperature sensor, a digital MEMS microphone and the BlueNRG-232 Bluetooth Low Energy application processor compliant with the Bluetooth 5.0 standard.
BlueNRG-Tile can be used as a sensing and connectivity hub for developing products such as wearables, gaming accesories, tracking systems, tags and smart home IoT devices.
You will learn:
- How to use the BlueNRG-Tile kit to quickly develop a Bluetooth Low Energy smart sensor node prototype
- To create a Bluetooth Low Energy smart sensor datalogger using the BlueNRG-Tile board and its companion "ST BLE Sensor" app for smartphones and tablets (Android and iOS)
- How to easily integrate sensor fusion algorithms into your sensor node design
- To upgrade firmware over-the-air (OTA) using Bluetooth Low Energy and a mobile app
Speaker
![]() |
Hary Radakichenane is a Senior Product Marketing Manager at STMicroelectronics. He began his career at ST in 1995 in Tours, France. In 1998, he transferred to the U.S. to work as a Product Marketing Engineer for ST's North America Distribution network. Since 2016, he has been Senior Product Marketing Manager for ST’s RF business unit in the Americas, based in the Dallas area. Hary was born in Paris, France and graduated from Universite de Bordeaux with a Master degree in Electronics and Semiconductors. |
Product Details
The STEVAL-BCN002V1B Bluetooth Low Energy enabled sensor node development kit features the STEVAL-BCN002V1 multi-sensor board based on BlueNRG-2 SoC Bluetooth Low Energy application processor. This sensor board includes an accelerometer, gyroscope, magnetometer, pressure, humidity, Time-of-Flight and microphone sensors, and is powered by a common CR2032 coin battery.
The sensor board communicates with a Bluetooth Low Energy enabled smartphone running the ST BLE Sensor app, available on Google Play and iTunes stores. The STEVAL-BCN002V1D adapter board is used to program and debug the sensor board. The adapter board is powered via USB.