On-demand Webinar: STM32WL, the most versatile SubGHz SoC


1-hour on-demand webinar to know all about the new, full featured single- and dual-core STM32WL wireless SoCs

► Recorded on December 2020


Further to the mass-market availability of STM32WL wireless SoCs, we hosted this webinar to showcase the features and industry-leading IP that is integrated into this market-unique LoRa-enabled SoC.

The STM32WL is the perfect choice for remote environmental sensors, meters, trackers and process controllers. 

The STM32WL SoC combines an ultra-low-power microcontroller and LoRa-compliant sub-GHz radio transceiver on the same chip for long-range IoT communication across sub-GHz bands.

Multiple modulation schemes also enable other wireless protocols such as SigFox and proprietary protocols. The radio stack and all branded protocol stacks are available free-of-charge.

Every STM32WL includes root-of-trust functions that ensure IoT security, and parts qualified to 105’C are available for operation in harsh industrial environments.

You will learn

  • About the industry-leading technology modulations supported in the STM32WL, which includes LoRa, Sigfox, FSK, MSK
  • What makes the single-core and dual-core STM32WL SoCs unique in the market
  • The benefits of the security and low-power features of the STM32WL
  • Ecosystem advantages of the STM32WL including wireless communication stacks supported today, debugging tools and the value-added features offered by ST

Agenda

  • Introduction to the STM32WL
  • Overview of STM32WL flexible architecture
  • Application use cases for the STM32WL
  • Power architecture overview
  • Security features and benefits inside the STM32WL
  • Communication stacks supported today on the STM32WL
  • STM32WL Ecosystem overview

There is a 20-minutes recorded Q&A session where our experts answered questions from the floor.

 

ST将保留您的浏览记录,并使用您以前访问、购买或下载过的产品和服务的详细信息,为您提供ST认为您也会感兴趣的其他产品和服务建议。
ST使用您直接提供的个人数据以及您在ST网站上的活动,并根据隐私政策向您发送(直接或通过ST分公司或分销商)有关ST产品和服务的电子报、广告或其他特定和有针对性的营销材料。您的个人资料将提供给位于欧盟和欧盟以外国家的ST分公司和分销商。您可以在我们网站的隐私政策中查阅ST分公司和分销商的列表。为了向您发送特定且有针对性的营销材料,我们会基于您直接向ST和/或通过您在ST网站上的活动提供的信息,或ST在其他情况下从您获得的其他信息进行综合分析(例如,如果您与ST、其分公司或分销商建立业务关系)。

 

Get started:

Speaker

Colin Ramrattan has been with STMicroelectronics since 2012 and is a Product Marketing Engineer with the microcontroller product marketing team for the Americas. Colin has held positions in both the analog sensors and connectivity organization previous to microcontrollers. Prior to ST, Colin was a user-interface module designer at Blackberry in Waterloo, Canada.