STSW-STM32095

NRND

用于STM32配置和初始化C代码生成的STM32CubeMX Eclipse插件

获取软件 下载数据摘要
概述
样片和购买
解决方案
文件
工具与软件
质量与可靠性
eDesignSuite
开始
Partner products
Sales Briefcase

产品概述

描述

STM32CubeMX is part of STMicroelectronics STMCubeoriginal initiative to ease developers life by reducing development efforts, time and cost. STM32Cube covers STM32 portfolio. STM32Cube includes the STM32CubeMX which is a graphical software configuration tool that allows generating C initialization code, using graphical wizards.
It also embeds a comprehensive software platform, delivered per series (such as STM32CubeF4 for STM32F4 series). This platform includes the STM32Cube HAL (an STM32 abstraction layer embedded software, ensuring maximized portability across STM32 portfolio), plus a consistent set of middleware components (RTOS, USB, TCP/IP and graphics). All embedded software utilities come with a full set of examples.
STM32CubeMX is an extension of the existing MicroXplorer tool. It is a graphical tool that allows configuring STM32 microcontrollers very easily and generating the corresponding initialization C code through a step-by-step process.
Step one consists in selecting the STMicroelectronics STM32 microcontroller that matches the required set of peripherals.
The user must then configure each required embedded software thanks to a pinout-conflict solver, a clock-tree setting helper, a power-consumption calculator, and a utility performing MCU peripheral configuration (GPIO, USART,...) and middleware stacks (USB, TCP/IP,...).
Finally, the user launches the generation of the initialization C code based on the selected configuration. This code is ready to be used within several development environments. The user code is kept at the next code generation.
  • 所有功能

    • Intuitive STM32 microcontroller selection
    • Microcontroller graphical configuration:
      • Pinout with automatic conflict resolution
      • Clock tree with dynamic validation of configuration
      • Peripherals and middleware functional modes and initialization with dynamic validation of parameter constraints
      • Power sequence with estimate of consumption results
    • C code project generation covering STM32 microcontroller initialization compliant with IAR, Keil®and GCC compilers
    • Available standalone or through Eclipse plug-in

获取软件

您可能还会喜欢...

特别推荐

All tools & software

    • 产品型号
      状态
      描述
      类型
      供应商

      STM32CubeIDE

      批量生产

      STM32的集成开发环境

      STM32软件开发套件 ST
      STM32CubeIDE

      描述:

      STM32的集成开发环境

      STM32CubeMX

      批量生产

      STM32Cube初始化代码生成器

      STM32配置程序和代码生成器 ST
      STM32CubeMX

      描述:

      STM32Cube初始化代码生成器