FLASHER-STM32

NRND

STM32 Flash加载器演示程序(UM0462)

获取软件 下载数据摘要
概述
样片和购买
解决方案
文件
工具与软件
质量与可靠性
eDesignSuite
开始
Partner products
Sales Briefcase

产品概述

描述

The STM32 Flash loader demonstrator (FLASHER-STM32) is a free software PC utility from STMicroelectronics, which runs on Microsoft® OSs and communicates through the RS232 with the STM32 system memory bootloader. To get an example of how to execute the device bootloader, refer to the STM32 microcontroller system memory boot mode Application note (AN2606). To get information about the USART protocol used in the STM32 bootloader, refer to the USART protocol used in the STM32 bootloader Application note (AN3155). This software utility contains also a command line version and it is provided with Microsoft®Visual Studio 12 source code.

获取软件

特别推荐