STSW-BLUENRG1-DK

批量生产

BlueNRG-1、BlueNRG-2 DK软件包

获取软件 下载数据摘要
概述
样片和购买
解决方案
文件
工具与软件
质量与可靠性
eDesignSuite
开始
Partner products
Sales Briefcase

产品概述

描述

The STSW-BLUENRG1-DK evaluation SW package is based on the BlueNRG-1 and BlueNRG-2 very low power Bluetooth low energy (BLE) single-mode systems-on-chip with 160 KB and 256 KB of Flash memory, respectively, 24 KB of RAM, 32-bit core ARM® Cortex®-M0 and ADC, GPIOs, I²C, RTC, SPI, Timers, UART, WDG and RTC peripherals. The STSW-BLUENRG1-DK SW package supports the BlueNRG-1 and BlueNRG-2 kit platforms available on relative web pages. It provides a Bluetooth low energy binary library with a complete set of APIs and related events callbacks allowing to interface with the Bluetooth low energy features offered by the BlueNRG-1 and BlueNRG-2 devices. The SW package also provides a set of BLE demonstration applications regarding some typical Bluetooth low energy working scenarios. Each demonstration application comes with a complete set of header and source files.
The STSW-BLUENRG1-DK SW package contains a complete set of peripheral drivers (header and source files), which allow to interface with the device peripherals (ADC, GPIOs,I²C, RTC, SPI, Timers, UART and WDG, RTC) and the Radio low level driver which provides access to the BlueNRG-1 2.4 GHz proprietary radio to send and receive packets without using the Bluetooth link layer.
The 2.4 GHz proprietary radio examples are built on top of the Radio Low level driver and can be used as reference examples for building other applications that use the BlueNRG-1 2.4 GHz proprietary radio.
The software package also includes BlueNRG-1 and BlueNRG-2 Navigator PC applications, which provide an interactive, simple and user-friendly interface to select and run demonstration applications for the resources available in the BlueNRG-1 and BlueNRG-2 DK SW packages, without the need for any extra hardware. The BlueNRG-1 and BlueNRG-2 Navigator are two instances of the same application tailored for the respective device, allowing access to the relative HW and SW kit resources available.
Another available PC application is the BlueNRG-X Radio Initialization Parameters Wizard that allows the definition of the proper values required for correct BlueNRG-1 and BlueNRG-2 BLE radio initialization, based on the specific user application scenario. A configuration header file, generated from the chosen parameter values, must then be used in the specific user software application folder.
  • 所有功能

    • Bluetooth® SMART SW package supporting BlueNRG-1 and BlueNRG-2 Bluetooth® low energy (BLE) systems-on-chip
    • BlueNRG-1 Navigator and BlueNRG-2 Navigator PC applications
    • BlueNRG-X Radio Initialization Parameters Wizard
    • Bluetooth low energy stack binary library and APIs, events callbacks interface
    • BlueNRG-1 and BlueNRG-2 Bluetooth low energy demonstration applications
    • BlueNRG-1 and BlueNRG-2 CMSIS files
    • BlueNRG-1 and BlueNRG-2 peripheral drivers and related examples
    • BlueNRG-1, BlueNRG-2 2.4 GHz radio proprietary driver and examples
    • BlueNRG-1 and BlueNRG-2 SDK and HAL drivers
    • BlueNRG-1 and BlueNRG-2 kit platforms support

获取软件

您可能还会喜欢...

特别推荐

All tools & software

    • 产品型号
      状态
      描述
      类型
      供应商

      STEVAL-IDB007V1M

      NRND

      基于SPBTLE-1S模块的评估平台

      通信和接口评估板 ST
      STEVAL-IDB007V1M

      描述:

      基于SPBTLE-1S模块的评估平台

      STEVAL-IDB007V2

      批量生产

      基于BlueNRG-1的STEVAL-IDB007V2评估平台

      通信和接口评估板 ST
      STEVAL-IDB007V2

      描述:

      基于BlueNRG-1的STEVAL-IDB007V2评估平台

      STEVAL-IDB008V1M

      批量生产

      BlueNRG-M2SAモジュールをベースにした開発ボード

      通信和接口评估板 ST
      STEVAL-IDB008V1M

      描述:

      BlueNRG-M2SAモジュールをベースにした開発ボード

      STEVAL-IDB008V2

      批量生产

      基于BlueNRG-2的评估平台

      通信和接口评估板 ST
      STEVAL-IDB008V2

      描述:

      基于BlueNRG-2的评估平台

      STEVAL-IDB009V1

      批量生产

      基于BlueNRG-248的评估平台

      通信和接口评估板 ST
      STEVAL-IDB009V1

      描述:

      基于BlueNRG-248的评估平台