X-CUBE-BAM

批量生产

STM32Cube的软件扩展,使用批采集模式(BAM)最大化功率效率(AN4515)

获取软件 下载数据摘要
概述
样片和购买
解决方案
文件
工具与软件
质量与可靠性
eDesignSuite
Partner products
Sales Briefcase

产品概述

描述

The X-CUBE-BAM embedded software describes an example of a BAM (batch acquisition mode) use case via a communication between an accelerometer and the STM32 microcontrollers. Once the user moves the accelerometer, the direction (UP or DOWN) is displayed via the PC.
In this use case the accelerometer exchanges data with the STM32 microcontroller via the I2C. During the data transfer, the MCU power consumption is reduced thanks to the use of the batch acquisition mode (BAM) feature offered by the STM32 microcontrollers.
This application case is monitored by a terminal display through the USB virtual comport communication between the MCU and the PC.
The embedded software package includes one project:
X-NUCLEO-IKS01A1: this project is based on a STM32 microcontroller (embedded in a STM32 Nucleo board) and an accelerometer (embedded in the STM32 Nucleo expansion board X-NUCLEO-IKS01A1).
The embedded software example is developed with the STM32Cube embedded software. It uses the EWARM, MDK-ARM™ and SW4STM32 toolchains and can be easily tailored for any other toolchain.
For more details refer to the application note AN4515.
  • 所有功能

    • Batch acquisition mode (BAM)
    • Sleep, Stop and Standby modes
    • Executing code from RAM
    • Low-power application case
    • Current consumption measurement

获取软件

特别推荐