X-CUBE-CLKTRIM

批量生产

使用STM32WB系列产品的RF应用HSE微调,STM32Cube的软件扩展

获取软件 下载数据摘要
概述
样片和购买
解决方案
文件
工具与软件
质量与可靠性
eDesignSuite
Partner products
Sales Briefcase

产品概述

描述

The X-CUBE-CLKTRIM Expansion Package illustrates the trimming of an HSE crystal oscillator to reach the high-accuracy frequency required by RF applications. The STM32WB Series microcontrollers support low-power RF standards such as Bluetooth® Low Energy (±50 ppm minimum HSE clock accuracy) and IEEE 802.15.4 (±40 ppm minimum HSE clock accuracy).
The STM32WL Series microcontrollers support sub-GHz RF standards such as LoRaWAN® and other low-power wide area networks (LPWAN). For these standards, the highest the HSE clock accuracy, the best the RF performance.
The frequencies of STM32 Wireless MCUs HSE oscillators can be tuned by means of values saved in dedicated registers. This features saves the extra cost of additional external capacitors and enables the compensation for frequency variations due to production, crystal, and PCB design.
The X-CUBE-CLKTRIM Expansion Package and associated application note (AN5042, AN5515) propose three different trimming procedures (manual, automatic, and with STM32CubeMonitor-RF (STM32CubeMonRF)) for the once-for-all storage of the right trimming parameters in OTP bytes. Each proposes two configurations: the trimming procedure itself and an implementation example of oscillator clock initialization in applications (loading of the trimming parameters in the according registers).
The HSE trimming manual procedure requires the user to use buttons to trim the RF clock frequency, which is output on a pin and can be monitored with a precision frequency meter. The HSE trimming automatic procedure consists in providing a precision clock reference to the STM32 so that it can trim its RF clock frequency (HSE) automatically. The HSE trimming procedure with STM32CubeMonitor-RF is similar to the manual one but uses STM32CubeMonitor-RF scripts instead of buttons.
For HSE trimming, it is not mandatory to trim each board in a production chain. A procedure is given for this purpose in the Precise HSE frequency trimming using STM32 wireless MCUs application note (AN5042).
X-CUBE-CLKTRIM firmware is built on the HAL drivers and runs on the Nucleo boards of the STM32 Wireless MCUs.
  • 所有功能

    • STM32 Wireless MCUs high-speed external (HSE) crystal oscillator trimming allowing best RF performance for Bluetooth® Low Energy, IEEE 802.15.4, LoRaWAN® and LPWAN wireless applications
    • Trimming parameters can be stored in user OTP Flash area
    • Trimming in production procedure suggestion

获取软件

您可能还会喜欢...

特别推荐

All tools & software

    • 产品型号
      状态
      描述
      类型
      供应商

      STM32CubeWB

      批量生产

      STM32Cube MCU包,用于STM32WB系列(HAL、LL底层驱动、USB、File system和RTOS - 附带在以下ST板上运行的示例:STM32 Nucleo、探索套件和评估板)

      STM32Cube MCU和MPU包 ST
      STM32CubeWB

      描述:

      STM32Cube MCU包,用于STM32WB系列(HAL、LL底层驱动、USB、File system和RTOS - 附带在以下ST板上运行的示例:STM32 Nucleo、探索套件和评估板)

      STM32CubeWL

      批量生产

      STM32Cube MCU Package for STM32WL series (HAL, Low-Layer APIs and CMSIS, File system, RTOS, KMS, Secure Engine, Sub-GHz Phy, LoRaWAN and Sigfox stacks - and examples running on ST boards)

      STM32Cube MCU和MPU包 ST
      STM32CubeWL

      描述:

      STM32Cube MCU Package for STM32WL series (HAL, Low-Layer APIs and CMSIS, File system, RTOS, KMS, Secure Engine, Sub-GHz Phy, LoRaWAN and Sigfox stacks - and examples running on ST boards)
    • 产品型号
      状态
      描述
      类型
      供应商

      NUCLEO-WL55JC

      批量生产

      STM32 Nucleo-64 development board with STM32WL55JCI MCU, SMPS, supports Arduino and morpho connectivity

      STM32 Nucleo 板 ST
      NUCLEO-WL55JC

      描述:

      STM32 Nucleo-64 development board with STM32WL55JCI MCU, SMPS, supports Arduino and morpho connectivity

      P-NUCLEO-WB55

      批量生产

      Bluetooth™ 5和802.15.4 Nucleo套件,包含USB dongle和采用STM32WB55 MCU的Nucleo-68,支持Arduino™ Uno V3和ST morpho连接

      STM32 Nucleo 扩充板 ST
      P-NUCLEO-WB55

      描述:

      Bluetooth™ 5和802.15.4 Nucleo套件,包含USB dongle和采用STM32WB55 MCU的Nucleo-68,支持Arduino™ Uno V3和ST morpho连接