X-CUBE-DBFU

批量生产

双存储区STM32微控制器的即时固件更新(AN4767)

获取软件 下载数据摘要
概述
样片和购买
解决方案
文件
工具与软件
质量与可靠性
eDesignSuite
Partner products
Sales Briefcase

产品概述

描述

The X-CUBE-DBFU Expansion Package is a project example that demonstrates an implementation of the on-the-fly firmware update on STM32 microcontrollers with a dual-bank Flash memory. The advantages of this feature are detailed in the On-the-fly firmware update for dual bank STM32 microcontrollers application note (AN4767), available on www.st.com.
  • 所有功能

    • Firmware upgrade example
    • Optional symmetric encryption on supported devices
    • Automatic and manual bank selection
    • Vector table relocation
    • Using YMODEM RS-232 for binary loading

获取软件

特别推荐