X-CUBE-FPUDEMO

批量生产

STM32微控制器上的浮点单元演示,STM32Cube的软件扩展(AN4044)

获取软件 下载数据摘要
概述
样片和购买
解决方案
文件
工具与软件
质量与可靠性
eDesignSuite
开始
Partner products
Sales Briefcase

产品概述

描述

This firmware package (X-CUBE-FPUDEMO) demonstrates the usage of the floating-point units (FPUs) available in the STM32 microcontrollers based on Cortex®-M4 and -M7 cores.It includes the implementation of the Julia-set and Mandelbrot-set algorithms to highlight the performances on the STM32 microcontrollers, but also to show the added value of the double-precision FPU on the STM32 microcontrollers based on Cortex®-M7 core. Choosing Julia-set gives the user an indication of the performances of the STM32 microcontrollers based on Cortex®-M4 and -M7 cores.Choosing Mandelbrot-set gives the user an indication about the gain in precision of the double-precision FPU on the STM32 microcontrollers based on Cortex®-M7 core.
This application is developed with the STM32Cube embedded software. It uses the IAR: EWARM, the ARM®Keil®: MDK-ARM and the free AC6: SW4STM32 tool chains and it can be easily tailored for any other tool chain.
  • 所有功能

    • Floating-point unit (SP FPU) in single precision
    • Floating-point unit (DP FPU) in double precision
    • Julia-set
    • Mandelbrot-set

获取软件

特别推荐

ST最新信息