X-CUBE-RC-CALIB

批量生产

STM32Cube的STM32L0和STM32L4校准软件扩展(AN4631和AN4736)

获取软件 下载数据摘要
概述
样片和购买
解决方案
文件
工具与软件
质量与可靠性
eDesignSuite
开始
Partner products
Sales Briefcase

产品概述

描述

The software package called X-CUBE-RC-CALIB, describes how to measure and calibrate internal oscillators. It also describes which internal features are used for calibration or measurement. Each oscillator trimming functionality is implemented in a separate file, so that users can easily select the file they need, without using the whole software package.
The software package X-CUBE-RC-CALIB is built on top of the STM32Cube HAL layer drivers.
For more details refer to the application notes “How to calibrate an STM32L0xx internal RC oscillator” (AN4631) and “How to calibrate STM32L4 Series microcontrollers internal RC oscillator” (AN4736).
  • 所有功能

    • STM32L0xx:
      • Calibrated oscillators: HSI16, MSI, HSI48
      • Measured oscillator: LSI
    • STM32L4xx:
      • Calibrated oscillators: HSI16, MSI, HSI48 (only for STM32L432 line)
      • Measured oscillator: LSI

获取软件

特别推荐