STSW-ST25R004

批量生产

ST25R NFC/HF读写器系列的天线匹配工具

获取软件 下载数据摘要
概述
样片和购买
解决方案
文件
工具与软件
质量与可靠性
eDesignSuite
开始
Partner products
Sales Briefcase

产品概述

描述

STSW-ST25R004 contains a graphical user interface (GUI) to specify the antenna parameters and the target matching. It performs transient, AC, and S-parameter simulations of the calculated antenna schematic. AN4974 and AN5276 (both available on ST website) provide guidance on the measurement of the antenna parameters required as input for this matching tool. With these inputs a best matching circuit can be defined.
  • 所有功能

    • STSW-ST25R004 is a software that calculates the matching network for antennas connected to ST25R3911B/ST25R391x devices, using Qucs (Quite Universal Circuit Simulator) to simulate the antenna and matching network characteristics.
    • The software supports the following products:
      • ST25R3910
      • ST25R3911
      • ST25R3911B
      • ST25R3912
      • ST25R3913
      • ST25R3914
      • ST25R3915
      • ST25R3916
      • ST25R3917

获取软件

特别推荐