X-CUBE-TIM-32RES

量産中

STM32Cube expansion software achieving 32-bit timer resolution by using the link system (AN2592)

ソフトウェア入手 データブリーフのダウンロード
概要
サンプル & 購入
ソリューション
ドキュメント
ツール & ソフトウェア
品質 & 信頼性
eDesignSuite
はじめる
Partner products
Sales Briefcase

製品概要

概要

The X-CUBE-TIM-32RES embedded software package is an expansion of the STM32Cube embedded software libraries. This firmware provides application use cases for the general-purpose-timer peripherals embedded in the STM32 microcontrollers.
The timers in microcontrollers can be linked together internally for timer synchronization or chaining purposes.
The X-CUBE-TIM-32RES describes how to use the link system to achieve the 32-bit resolution with two 16-bit timers.
For more details refer to Achieving 32-bit timer resolution with software expansion for STM32Cube and Standard Peripheral Library application note (AN2592).
  • 特徴

    • 32-bit input capture mode example using link system
    • 32-bit input capture mode example using one timer only
    • Two 32-bit output capture mode examples using link system
      • Active mode
      • Toggle mode
    • Microcontrollers covered: STM32F1 Series and STM32L0 Series

ソフトウェア入手

推奨コンテンツ