ソリューション概要
The AEKD-USBTYPEC1 demo kit allows for the evaluation of the USB Power Delivery protocol stack version 2.0 implemented on the ASIL-B automotive grade 32-bit Power Architecture® microcontroller.
The kit is composed of the following boards: SPC58 MCU board with CAN, LIN, Ethernet among others and an interface board hosting two USB Type-C controllers (STUSB1702) for two separate ports. On top of the interface board, a specific connector is provided for external power boards able to extend available power profiles (PDOs). Together with this, an easily customizable software is provided: the software runs parallel tasks on a free real-time operating system (RTOS).
The AEKD-USBTYPEC1 kit is composed of
- SPC58EC-DISP Microcontroller discovery board
- AEK-USB-2TYPEC1 dual port USB Type-C interface board with a pair of STUSB1702Y automotive grade USB Type-C controllers
- STSW-USB2TYPEC1 firmware (MCU flash image).
The kit is very flexible, scalable, customizable and automotive grade compliant. Through the Microcontroller Discovery board, you can expand your application by connecting additional boards.
The SPC58EC-DISP discovery board hosts SPC58 ASIL-B automotive grade 32-bit Power Architecture microcontroller with, CAN ports, Flex port and Ethernet port among others. The microcontroller pins are multi-functions, i.e. through internal microcontroller register programming, it is possible to assign different functionalities to the same pin. The capability of SPC5 to configure its pins and the intuitive graphical interface of SPC5 Studio development environment are key elements for fast-prototyping and customizable application design.
The functional interface board, AEK-USB-2TYPEC1, hosts a pair of STUSB1702Y, automotive grade USB Type-C controller with TX/RX line driver and BMC, one for each USB Type-C port. The board contains devices for ESD protection, dual Transil™ array ESDA25LY and very low capacitance USBLC6-2SC6Y. The ports status are monitored on the board through some LEDs. One of this LED (the green one on each port) will turn-on once the power profile negotiation is successfully reached between provider and consumer.
The firmware STSW-USB2TYPEC1 is pre-loaded on the SPC58EC-DISP discovery board and it is available for download from ST.COM after registration.
In addition to the STSW-USB2TYPEC1 firmware, the following software is available:
- A driver dedicated to the STUSB1702Y device
- An SPC5 Studio plugin for the USB Power Delivery software stack
- A demo application
The software can be configured via SPC5 Studio dedicated plugin for USB-PD stack without the need for coding but just by automatically re-generating the code.
Estimated cost
サーバへのリクエストに失敗しました。しばらくしてから再度お試しください
リクエストを送信しました。48時間以内にリクエストの承認メールをお送りします。メール内のリンクからリクエストされたソフトウェアをダウンロードしてください。
Unfortunately, the link you clicked didn't work. Don't worry, here are the steps you can take to get your download started:
If you still can't download the software, please reach out to us on the ST Community and we will help you- Ensure you are using the same browser used to made the initial request
- Check that cookies are allowed in your browser
- Update your browser to its latest version
- Please also note that links forwarded by somebody else will not work
ソフトウェアを入手
製品型番 | 概要 | Marketing Status | ダウンロード |
---|---|---|---|
STSW-USB2TYPEC1 | AEKD-USBTYPEC1 kit software package for automotive USB Type-C™ and Power Delivery dual port applications | Active | x ソフトウェア入手 ご登録ありがとうございました サーバへのリクエストに失敗しました。しばらくしてから再度お試しください my.st.comのアカウントをお持ちの場合は、ログイン後、認証手続きをせずにソフトウェアをダウンロードしていただけます。 ログインを希望されない場合でも、お名前とメールアドレスを下のフォームに入力し、確定していただくだけで、ソフトウェアをダウンロードすることが可能です。 これにより、STはお客様への継続的な情報提供が可能となり、本ソフトウェアの更新についてお知らせすることができます。 さらにダウンロードを続ける場合、多くのソフトウェアについては、この手順をもう一度行う必要はありません。 To validate your e-mail and start the download, please click on the link inside the e-mail that has been sent to you. This link will be valid for 24 hours. Please check your spam filters in case you did not receive the e-mail. x E-mail not yet validated The e-mail address that you have entered during the download attempt has not yet been validated. Please check your inbox for the e-mail with the download link. In case you did not receive the e-mail, or you entered a wrong e-mail address, you can start-over the process. x About Requesting Software
x ライセンス契約同意Unless otherwise expressly stipulated under Article 1, You shall not, and shall not permit any third party to: (i) copy, reproduce or duplicate the Licensed Materials; (ii) translate, modify, adapt, decompile, disassemble or reverse engineer and make derivative works of all or any portion of the Licensed Materials; (iii) rent, disclose, publish, sell, assign, lease, lend, sublicense, market, transfer, distribute or otherwise provide third parties access to (any portion of) the Licensed Materials for any purpose; (iv) attempt to derive the source code, algorithmic nature or structure of any object code portions of the Licensed Materials; (v) use the Licensed Materials to create any product that competes with the Licensed Materials or ST Products; (vi) remove or circumvent any protection or other restrictive technology mechanism of the Licensed Materials or ST Products; (vii) disclose the results of the Licensed Materials’ performance benchmarks to any third party; or (viii) otherwise use (any portion of) the Licensed Materials in any manner not expressly authorized by this PLLA. Other than the limited expressed license granted to You under Article 1 herein, no other rights or licenses are granted, or implied by estoppel or otherwise, under any intellectual property rights of ST and/or its Affiliates or any intellectual property of a third-party residing in the Licensed Materials or any other confidential information furnished by ST and its Affiliates, including (i) for the combination of such Licensed Materials or other confidential information with one or more other items (including items acquired from ST and/or its Affiliates) even if such items have no substantial use other than as part of such combination (ii) with respect to any trademark, trade or brand name, a corporate name of ST and/or its Affiliates, or any other name or mark, or contraction abbreviation or simulation thereof, (iii) under any intellectual property rights covering any standard set by a standard setting body and any de facto standards. ST and its Affiliates have no obligation to provide You with maintenance, support or updates for the Licensed Materials. Nothing in this PLLA will be construed as: (i) a warranty or representation by ST and its Affiliates to maintain production of any ST software or ST Product with which the Licensed Materials may be used in any manner; and (ii) a commitment from ST and its Affiliates to bring or prosecute actions against third-parties for infringement. You shall limit access and use of the Licensed Materials to You and those individuals who may be employed by You who have a need to access the Licensed Materials for the purpose of this PLLA and provided that You shall ensure that such individuals shall comply with the provisions of this PLLA, and except as expressly permitted under Article 1 or as otherwise expressly agreed in writing by ST, You shall not allow any third-party to use the Licensed Materials, You shall be liable towards ST for any damages due to a failure by such third-party(ies) to comply with the provisions of this PLLA. The Licensed Materials are and will remain the exclusive property of ST and/or its Affiliates or its licensors, whether or not specifically recognized or perfected under the laws of the country where the Licensed Materials are used. You will not take any action that jeopardizes ST and its Affiliates or its licensors' proprietary rights or acquire any rights in the Licensed Materials, except the limited rights specified in Article 1. All rights, titles, and interests in and to the Licensed Materials are owned or licensed by ST, its Affiliates and suppliers. You shall ensure that all notices, including but not limited to all copyright and trademark notices of ST or its Affiliates or licensors are reproduced in any copy of the whole or any part of the Licensed Materials. You shall not remove, modify or alter any ST or its Affiliates’ or licensors’ copyright or trademark notice from any part of the Licensed Materials. Confidential information shall include all information provided with the Licensed Materials which (a) is designated as “confidential”, “proprietary” or with a similar legend, (b) is by its own nature of a type which would reasonably be considered confidential and/or (c) is source code (“Confidential Information”). You may only use the Confidential Information for the purpose of this PLLA and shall protect the confidentiality of the Confidential Information provided by ST and its Affiliates under this PLLA by using the same degree of care, but not less than a reasonable degree of care, to prevent its unauthorized use, dissemination, or publication as You use to protect your own confidential information of like nature. You shall be liable towards ST for any damages incurred due to a failure by any employee, third party contractor or customer having access to the Licensed Materials and/or the Confidential Information to comply with the provisions in this PLLA. You shall immediately notify ST of any unauthorised use or disclosure of, or of any unauthorised access to, or of any theft or loss of the Licensed Materials or Confidential Information or part thereof, which comes to your notice. The confidentiality obligations shall not apply to Confidential Information, which can be shown by documentary evidence: (i) entered the public domain through no fault of the Licensee; or, (ii) was known to the Licensee prior to receipt from ST and its Affiliates; or, (iii) was disclosed to the Licensee by a third party having the right to disclose; or, (iv) was independently developed by the Licensee without use of the Licensed Materials or the Confidential Information, the onus of proof of independence being on the Licensee. These confidentiality obligations shall survive any termination or expiration of the PLLA for whatever cause. YOU ACKNOWLEDGE THAT THE LICENSED MATERIALS AND ANY AND ALL PARTS THEREOF ARE PROVIDED “AS IS”. ST AND ITS AFFILIATE MAKE NO REPRESENTATIONS OR WARRANTIES WITH RESPECT TO THE LICENSED MATERIALS AND OR PARTS THEREOF WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING BUT NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE. SPECIFICALLY, WITHOUT LIMITING THE GENERALITY OF THE FOREGOING, ST AND ITS AFFILIATES MAKE NO REPRESENTATION OR WARRANTY THAT (I) THE USE AND DISTRIBUTION OF THE LICENSED MATERIALS AND OR PARTS THEREOF WILL BE UNINTERRUPTED OR ERROR FREE, AND OR (II) ANY USE AND DISTRIBUTION OF THE LICENSED MATERIALS AND OR PARTS THEREOF, WHETHER INTEGRATED INTO OTHER EQUIPMENT OR NOT, ARE FREE FROM INFRINGEMENT OF ANY THIRD PARTY INTELLECTUAL PROPERTY RIGHTS. IT SHALL BE YOUR SOLE RESPONSIBILITY TO MAKE SUCH DETERMINATION AS NECESSARY WITH RESPECT TO THE ACQUISITION OF LICENSES UNDER PATENTS AND OTHER INTELLECTUAL PROPERTY RIGHTS OF THIRD PARTIES. CONSEQUENTLY, ST AND ITS AFFILIATES DISCLAIM ANY LIABILITY IN CASE ANY SUCH USE AND DISTRIBUTION INFRINGE ANY THIRD PARTY’S INTELLECTUAL PROPERTY RIGHTS. FURTHERMORE ST AND ITS AFFILIATES HEREBY DISCLAIM ANY WARRANTY AND LIABILITY WHATSOEVER FOR ANY DEVELOPMENT CREATED BY OR FOR YOU OR YOUR CUSTOMERS. YOU ACKNOWLEDGE THAT YOU HAVE RELIED ON NO WARRANTIES AND THAT NO WARRANTIES ARE MADE BY ST AND ITS AFFILIATES OR GRANTED BY LAW WHENEVER IT IS PERMITTED BY LAW. Some portion of the Licensed Materials might contain Open Source Software subject to Open Source Terms (as defined below) applicable for each such portion, as further specified in the Licensed Materials. Such Open Source Software is supplied to You under the applicable Open Source Terms and is not subject to the terms of this PLLA to the extent the terms of this PLLA are in conflict with such applicable Open Source Terms. Except for Open Source Software, You have no rights under this PLLA to, and may not under any circumstances use the Licensed Materials or any parts thereof such that they become subject to any Open Source Terms. These actions include but are not limited to combining the Licensed Materials by means of incorporation or linking or otherwise. For the purpose of this PLLA, “Open Source Terms” shall mean any open source license which requires as part of distribution of software that the source code of such software is distributed therewith, or open source license that complies with the Open Source Definition specified at www.opensource.org and any other comparable open source license such as for example GNU General Public License (GPL), Eclipse Public License (EPL), Apache Software License, BSD license and MIT license. “Open Source Software” shall mean any software that is licensed or distributed under Open Source Terms as specified in the Licensed Materials. You agree not to use the Licensed Materials in violation of any applicable law, statute, ordinance or other regulation or any obligation by which You are bound. You agree to comply with all applicable laws and regulations affecting the use of the Licensed Materials. Specifically but without limiting the generality of the foregoing, You acknowledge that the Licensed Materials are subject to export controls restrictions and You agree to comply with any applicable export control law or regulation including but not limited to the European export regulations and US similar regulations, and to obtain any necessary export license or other documentation prior to exportation or re-exportation of the Licensed Materials. Some Licensed Materials may (i) require licenses from third parties claiming intellectual property rights covering use or implementation of the Licensed Materials or (ii) be based on industry recognized standards or software programs published by industry recognized standards bodies and certain third parties may claim to own intellectual property rights that cover implementation or use of those standards. You agree that You are responsible for obtaining any such license which may be needed, and no such license is provided by ST or its Affiliates. You shall be responsible for the due and proper compliance with the terms and conditions of this PLLA by your customers and shall be liable to ST for any and all damages incurred by ST, its Affiliates and its suppliers and licensors in connection with any such customers’ non-compliance therewith. IN NO EVENT SHALL ST AND ITS AFFILIATES BE LIABLE TO THE LICENSEE AND ITS CUSTOMERS FOR ANY INDIRECT, INCIDENTAL, PUNITIVE, SPECIAL OR CONSEQUENTIAL DAMAGES, LOST PROFITS OR LOST SAVINGS, LOSS OF BARGAIN OR OPPORTUNITY, PROFESSIONAL FEES OR EXPENSES, BUSINESS INTERRUPTION, LOST REVENUES OR SALES, DAMAGE TO PRODUCT OR EQUIPMENT OR TO FACILITIES, COSTS OF SUBSTITUTE PRODUCT, FACILITIES OR SERVICES, REWORK CHARGES, COSTS ASSOCIATED WITH DOWN TIME, LOSS OF GOODWILL, LOSS OF DATA OR FOR ANY DAMAGES COSTS OR EXPENSES ASSOCIATED WITH WARRANTY OR INTELLECTUAL PROPERTY INFRINGEMENT CLAIMS, WHETHER FORESEEABLE OR UNFORESEEABLE AND WHETHER OR NOT SUCH DAMAGES ARE BASED ON WARRANTY, CONTRACT OR ANY OTHER LEGAL THEORY – EVEN IF LICENSEE HAS BEEN ADVISED, OR IS AWARE, OF THE POSSIBILITY OF SUCH DAMAGES ARISING FROM OR IN CONNECTION WITH THIS PLLA. ST AND ITS AFFILIATES AGGREGATE AND CUMULATIVE LIABILITY UNDER THIS PLLA SHALL NOT EXCEED 100 USD (ONE HUNDRED USD). THE LIMITATIONS SET FORTH IN THIS ARTICLE 8 SHALL ONLY APPLY TO THE MAXIMUM EXTENT PERMITTED BY APPLICABLE LAW. This PLLA shall be valid from acceptance by You of this PLLA for an unlimited period of time until terminated by either ST or Licensee upon one (1) month prior written notice to the other. Notwithstanding the foregoing, Licensee may terminate this PLLA at any time by destroying all Licensed Materials, Documentation and other Confidential Information or by returning those to ST. ST may terminate this PLLA at any time if (i) You fail to comply with the terms and conditions of this PLLA, or (ii) You file litigation against ST or its Affiliates, (iii) ST or its Affiliates receive notice of any claim, suit or proceeding that alleges that the Licensed Materials or Your use or distribution of the Licensed Materials infringes any third-party intellectual property rights or (iv) to the extent permitted by laws, a voluntary or involuntary petition in bankruptcy or winding up is filed against Licensee, any proceedings in insolvency or bankruptcy are instituted against Licensee, a trustee or receiver is appointed over Licensee, or any assignment is made for the benefit of creditors of Licensee. Upon termination You shall delete, destroy, or return to ST all Licensed Materials in your possession and You shall stop using the Licensed Materials for any purpose whatsoever. The rights and obligations under Articles from 2 to 11 will survive the termination of this PLLA. However the right to use the Licensed Materials incorporated in a Licensee Product as per Article 1 will survive with respect to Licensee Products sold, licensed or distributed before the termination of this PLLA. If a court or agency of competent jurisdiction holds any term of this PLLA invalid, illegal, or unenforceable for any reason, the remainder of this PLLA shall be valid and enforceable and You and ST shall discuss in good faith a substitute, valid, enforceable provision which most nearly effects the parties intent in entering into this PLLA. The failure by ST to enforce any provisions of this PLLA or to exercise any right in respect thereto shall not be construed as constituting a waiver of its rights thereof. No agency, joint venture, partnership or other business organisation shall be created or be construed as being created by reason of this PLLA. You will not have the right or authority to, and shall not, assume or create any obligation of any nature whatsoever on behalf of ST and its Affiliates or bind ST and its Affiliates in any respect whatsoever. You and ST are independent parties and nothing in this PLLA shall be construed as making You an employee, agent or legal representative of ST. This PLLA contains the entire and sole agreement between You and ST on the subject matter of this PLLA, and supersedes all representations, undertakings and agreements previously made between You and ST and/or its Affiliates and shall prevail over the terms and conditions set forth in any document from You with respect to the subject matter of this PLLA. Any amendment to this PLLA shall be agreed in writing and duly signed by You and ST or signed solely by You on the format proposed by ST and shall make reference to this PLLA. This PLLA is governed by the laws of Switzerland, without regard to its conflict of law rules. All disputes or questions arising out of or in connection with this PLLA shall be finally settled by the competent courts of Geneva, Switzerland. Notwithstanding the aforesaid, nothing in this PLLA shall prevent ST from seeking any interim or final injunctive or equitable relief by a court of competent jurisdiction. |
評価ボード概要
-
The functional interface board, AEK-USB-2TYPEC1, hosts a pair of STUSB1702Y, automotive grade USB Type-C controller with TX/RX line driver and BMC, one for each USB Type-C port. The board contains devices for ESD protection, dual Transil™ array ESDA25LY and very low capacitance USBLC6-2SC6Y. The ports status are monitored on the board through some LEDs. One of this LED (the green one on each port) will turn-on once the power profile negotiation is successfully reached between provider and consumer.
The firmware STSW-USB2TYPEC1 is pre-loaded on the SPC58EC-DISP discovery board and it is available for download after registration.
In addition to the STSW-USB2TYPEC1 firmware, the following software is available:
- A driver dedicated to the STUSB1702Y device
- An SPC5 Studio plugin for the USB Power Delivery software stack
- A demo application
- The software can be configured via SPC5 Studio.
アンプ & コンパレータ
製品型番 | 概要 |
---|---|
TSC1031 | High-voltage high side current sense amplifier |
Automotive Analog and Power
製品型番 | 概要 |
---|---|
L5963 | Automotive dual monolithic switching regulator with LDO and HSD |
Automotive Microcontrollers
製品型番 | 概要 |
---|---|
SPC58EC80E5 | 32-bit Power Architecture MCU for Automotive General Purpose Applications - Chorus family |
Interfaces and Transceivers
製品型番 | 概要 |
---|---|
STUSB1702 | USB Type-C controller (with Tx/Rx line driver and BMC) |
パワー・マネージメント
製品型番 | 概要 |
---|---|
A5973D | Up to 2 A step down switching regulator for automotive applications |
Power Transistors
製品型番 | 概要 |
---|---|
2STN1360 | Low voltage fast-switching NPN power transistors |
STD28P3LLH6AG | Automotive-grade P-channel -30 V, 0.027 Ohm typ., -12 A, STripFET H6 Power MOSFET in a DPAK package |
STD45P4LLF6AG | Automotive-grade P-channel -40 V, 12 mOhm typ., -50 A STripFET F6 Power MOSFET in a DPAK package |
STD95P3LLH6AG | Automotive-grade P-channel -30 V, 5 mOhm typ., -80 A, STripFET H6 Power MOSFET in a DPAK package |
Protection Devices
製品型番 | 概要 |
---|---|
ESDALY | Automotive dual Transil™ array for ESD protection |
HSP061-4M10Y | Automotive 4-line ESD protection for high speed lines |
SM4TY | Automotive 400 W TVS in SMA |
SM6TY | Automotive 600 W TVS in SMB |
USBLC6-2SC6Y | Automotive very low capacitance ESD protection |
EDA Symbols, Footprints and 3D Models
STMicroelectronics - SL-PRIPM09402V1
Speed up your design by downloading all the EDA symbols, footprints and 3D models for your application. You have access to a large number of CAD formats to fit with your design toolchain.

Symbols

Footprints

3D models