TVS智能选择器

概述
产品选择器
解决方案
文件
CAD资源
工具与软件
eDesignSuite
开始

The SEL-PROT-TVS transient voltage suppressor smart selection tool helps designers select the right TVS for their application with just a few clicks. Only two application parameters are necessary for device selection. 

The first parameter is the type of protection required, such as automotive, power line, analog or digital line. 

The second is the signal standard, e.g. CAN, USB, SD-Card, 10/1000 μs or custom. 

In addition, a restriction can be raised at protection level (ESD, power, peak current) and/or at package level.