STM32CubeMonUCPD

批量生产

用于STM32 USB-C和Power Delivery 3.0应用的监控和配置软件工具

获取软件 下载数据摘要
概述
样片和购买
解决方案
文件
工具与软件
质量与可靠性
eDesignSuite
开始
Partner products
Sales Briefcase

产品概述

描述

STM32CubeMonitor-UCPD (STM32CubeMonUCPD) is a free software analyzer to monitor and configure USB Type-C and Power Delivery applications. It applies to any STM32 microcontroller running ST USB PD middleware stack. The development and the debug are simplified by key messages of USB PD protocol accessible through a convivial user interface. The developer can visualize in-live status and capability of any USB Type-C port (such as sink, source, or dual-role port), and USB PD packet messages during contract negotiation. The user can interact with the application environment by sending USB PD commands to the target board. The power or data role swap is executed in one click. The selection or the creation of new sink or source power profiles is made simple. The monitoring of analog parameters such as VBUS or IBUS is displayed in a specific measurement pane to facilitate the debug of the final application while the in-live debug trace pane allows visualizing message exchanges between the two ports.
  • 所有功能

    • Monitoring and configuring tool for USB Type-C and USB Power Delivery applications using STM32 microcontroller
    • Support of USB Type-C 1.2 and USB PD 2.0/3.0 specifications
    • Multi-pane including:
      • Port configuration pane for Power Delivery (PD) setting, vendor defined messages (VDM), standard operating procedures (SOP), source and sink capabilities
      • Port communication pane for VBUS and IBUS monitoring, distant port capabilities, message selector, and real-time traces
    • Multi-OS support: Windows, Linux, and macOS
    • Multi-language support: English, Chinese, French, Arabic
    • GUI responder for communication between the target board and STM32CubeMonitor-UCPD

获取软件

更多产品线信息

您可能还会喜欢...

特别推荐

STM32MCU WIKI
discover STM32 software toolchain

All tools & software

    • 产品型号
      状态
      描述
      类型
      供应商

      STM32CubeG0

      批量生产

      STM32Cube MCU包,用于STM32G0系列(HAL、底层API和CMSIS(CORE、DSP和RTOS)、USB PD、File system和RTOS - 附带在以下ST板上运行的示例:STM32 Nucleo、探索套件和评估板)

      STM32Cube MCU和MPU包 ST
      STM32CubeG0

      描述:

      STM32Cube MCU包,用于STM32G0系列(HAL、底层API和CMSIS(CORE、DSP和RTOS)、USB PD、File system和RTOS - 附带在以下ST板上运行的示例:STM32 Nucleo、探索套件和评估板)
    • 产品型号
      状态
      描述
      类型
      供应商

      NUCLEO-G070RB

      批量生产

      采用STM32G070RB MCU的STM32 Nucleo-64开发板,支持Arduino和ST morpho连接

      STM32 Nucleo 板 ST
      NUCLEO-G070RB

      描述:

      采用STM32G070RB MCU的STM32 Nucleo-64开发板,支持Arduino和ST morpho连接

      NUCLEO-G071RB

      批量生产

      采用STM32G071RB MCU的STM32 Nucleo-64开发板,支持Arduino和ST morpho连接

      STM32 Nucleo 板 ST
      NUCLEO-G071RB

      描述:

      采用STM32G071RB MCU的STM32 Nucleo-64开发板,支持Arduino和ST morpho连接

      STM32G071B-DISCO

      批量生产

      探索套件,采用STM32G071RB MCU

      STM32发现工具包 ST
      STM32G071B-DISCO

      描述:

      探索套件,采用STM32G071RB MCU

      STM32G081B-EVAL

      批量生产

      评估板,采用STM32G081RB MCU

      STM32微控制器评估工具 ST
      STM32G081B-EVAL

      描述:

      评估板,采用STM32G081RB MCU
    • 产品型号
      状态
      描述
      类型
      供应商

      STM32CubeIDE

      批量生产

      STM32的集成开发环境

      STM32软件开发套件 ST
      STM32CubeIDE

      描述:

      STM32的集成开发环境

      STM32CubeMX

      批量生产

      STM32Cube初始化代码生成器

      STM32配置程序和代码生成器 ST
      STM32CubeMX

      描述:

      STM32Cube初始化代码生成器