X-CUBE-53L0A1

批量生产

STM32Cube的测距传感器软件扩展

获取软件 下载数据摘要
概述
样片和购买
解决方案
文件
工具与软件
质量与可靠性
eDesignSuite
Partner products
Sales Briefcase

产品概述

描述

The X-CUBE-53L0A1 software package is an expansion for STM32Cube, to go along with the X-NUCLEO-53L0A1 expansion board for STM32 Nucleo. The source code of this package is based on STM32Cube and is aligned with the “Multi-Platform” file & directory structure to ease portability and code sharing across different STM32 MCU families.
The VL53L0X is the latest product based on ST’s patented FlightSenseTMtechnology. This is a ground-breaking technology allowing absolute distance to be measured independent of target reflectance. Instead of estimating the distance by measuring the amount of light reflected back from the object (which is significantly influenced by color and surface), the VL53L0X precisely measures the time the light takes to travel to the nearest object and reflect back to the sensor (Time-of-Flight).
  • 所有功能

    • Driver layer (VL53L0X API) for complete management of the VL53L0X ranging and gesture detection sensor integrated in theX-NUCLEO-53L0A1 expansion board.
    • Easy portability across different MCU families, on the strength of STM32Cube.
    • Free, user-friendly license terms.
    • Example code for ranging measurement with typical settings in order to address most common use cases, like long range, high speed, high accuracy.
    • Example code for ranging with multiple VL53L0X sensors. Up to 3x VL53L0X devices can be controlled using the X-NUCLEO-53L0A1 expansion board equipped with 2x satellites.
    • Data logging capabilities through serial com over USB.
    • Example code of gesture recognition.

获取软件

您可能还会喜欢...

特别推荐

All tools & software

    • 产品型号
      状态
      描述
      类型
      供应商

      X-NUCLEO-53L0A1

      批量生产

      STM32 Nucleo的测距传感器扩展板,基于VL53L0X

      影像IC评估板 ST
      X-NUCLEO-53L0A1

      描述:

      STM32 Nucleo的测距传感器扩展板,基于VL53L0X
    • 产品型号
      状态
      描述
      类型
      供应商

      P-NUCLEO-53L0A1

      批量生产

      VL53L0X Nucleo Pack - Includes VL53L0X Expansion board and STM32F401RE Nucleo

      STM32 ODE检测硬件 ST
      P-NUCLEO-53L0A1

      描述:

      VL53L0X Nucleo Pack - Includes VL53L0X Expansion board and STM32F401RE Nucleo