X-CUBE-53L1A1

批量生产

STM32Cube的长距离测距传感器软件扩展

获取软件 下载数据摘要
概述
样片和购买
解决方案
文件
工具与软件
质量与可靠性
eDesignSuite
开始
Partner products
Sales Briefcase

产品概述

描述

The X-CUBE-53L1A1 software package is an expansion of the STM32Cube, to go with the X-NUCLEO-53L1A1 expansion board for STM32 Nucleo. The source code of this package is based on STM32Cube and is aligned with the “multi-platform” file and directory structure to ease portability and code sharing across different STM32 MCU families.
The VL53L1X is the latest product based on ST’s patented FlightSenseTM technology. This is a ground-breaking technology allowing absolute distance to be measured independent of target reflectance. Instead of estimating the distance by measuring the amount of light reflected back from the object (which is significantly influenced by color and surface), the VL53L1X precisely measures the time the light takes to travel to the nearest object and reflect back to the sensor Time-of-Flight (ToF).
  • 所有功能

    • Driver layer (VL53L1X API) for complete management of the VL53L1X long-distance ranging sensor integrated in theX-NUCLEO-53L1A1 expansion board
    • Easy portability across different MCU families, on the strength of STM32Cube
    • Free, user-friendly license terms
    • Example code for getting started with a simple ranging measurement
    • Data logging capabilities through serial com over USB.

获取软件

特别推荐