STM32CubeF4

批量生产

STM32Cube MCU包,用于STM32F4系列(HAL、底层API和CMSIS(CORE、DSP和RTOS)、USB、TCP/IP、File system、RTOS和Graphic - 附带在以下ST板上运行的示例:STM32 Nucleo、探索套件和评估板)

获取软件 下载数据摘要
概述
样片和购买
解决方案
文件
工具与软件
质量与可靠性
eDesignSuite
Partner products
Sales Briefcase

产品概述

描述

STM32Cube is an STMicroelectronics original initiative to significantly improve developer productivity by reducing development effort, time and cost. STM32Cube covers the whole STM32 portfolio.
STM32Cube includes STM32CubeMX, a graphical software configuration tool that allows the generation of C initialization code using graphical wizards.
It also comprises the STM32CubeF4 MCU Package composed of the STM32Cube hardware abstraction layer (HAL) and the low-layer (LL) APIs, plus a consistent set of middleware components (RTOS, USB, FAT file system, Graphics and TCP/IP). TouchGFX graphic software stack is also included in the STM32CubeF4 MCU Package as a part of the STM32Cube ecosystem. It is available free of charge for production and redistribution on STM32 microcontrollers. All embedded software utilities are delivered with a full set of examples running on STMicroelectronics boards.
The STM32Cube HAL is an STM32 embedded software layer that ensures maximized portability across the STM32 portfolio, while the LL APIs make up a fast, light-weight, expert-oriented layer which is closer to the hardware than the HAL. HAL and LL APIs can be used simultaneously with a few restrictions.
Both the HAL and LL APIs are production-ready and have been developed in compliance with MISRA-C®:2004 guidelines with some documented exceptions (reports available on demand) and ISO/TS 16949. Furthermore, ST-specific validation processes add a deeper-level qualification.
STM32CubeF4 gathers in one single package all the generic embedded software components required to develop an application on STM32F4 microcontrollers. Following STM32Cube initiative, this set of components is highly portable, not only within the STM32F4 Series but also to other STM32 Series. In addition, the low-layer APIs provide an alternative, high-performance, low-footprint solution to the STM32CubeF4 HAL at the cost of portability and simplicity.
HAL and LL APIs are available in open-source BSD license for user convenience.
  • 所有功能

    • Consistent and complete embedded software offer that frees the user from dependency issues
    • Maximized portability between all STM32 Series supported by STM32Cube
    • Hundreds of examples for easy understanding
    • High quality HAL and low-layer API drivers using CodeSonar® static analysis tool
    • TouchGFX graphics software stack
    • STM32F4-dedicated middleware including USB Host and Device, and TCP/IP
    • Free user-friendly license terms
    • Update mechanism that can be enabled by the user to be notified of new releases

获取软件

更多产品线信息

您可能还会喜欢...

特别推荐

All tools & software

    • 产品型号
      状态
      描述
      类型
      供应商

      X-CUBE-NFC2

      批量生产

      X-NUCLEO-NFC02A1的STM32Cube扩展软件

      STM32Cube扩展包 ST
      X-CUBE-NFC2

      描述:

      X-NUCLEO-NFC02A1的STM32Cube扩展软件

      X-CUBE-NFC3

      批量生产

      STM32Cube的13.56 MHz多协议非接触式收发器IC软件扩展

      STM32Cube扩展包 ST
      X-CUBE-NFC3

      描述:

      STM32Cube的13.56 MHz多协议非接触式收发器IC软件扩展
    • 产品型号
      状态
      描述
      类型
      供应商

      SPL2LL-Converter

      批量生产

      STM32标准外设库至STM32Cube底层API迁移工具

      STM32配置程序和代码生成器 ST
      SPL2LL-Converter

      描述:

      STM32标准外设库至STM32Cube底层API迁移工具

      STM32CubeMX

      批量生产

      STM32Cube初始化代码生成器

      STM32配置程序和代码生成器 ST
      STM32CubeMX

      描述:

      STM32Cube初始化代码生成器

      TouchGFXDesigner

      批量生产

      STM32 MCU的TouchGFX图形设计和代码生成工具

      STM32配置程序和代码生成器 ST
      TouchGFXDesigner

      描述:

      STM32 MCU的TouchGFX图形设计和代码生成工具
    • 产品型号
      状态
      描述
      类型
      供应商

      ST Trainings

      批量生产

      STM32、STM8和ST生态系统培训

      培训 MASTERS
      ST Trainings

      描述:

      STM32、STM8和ST生态系统培训