STSW-IMG008

批量生产

VL53L1X Nucleo包的Windows图形用户界面(GUI)。与P-NUCLEO-53L1A1配合使用。

获取软件 下载数据摘要
概述
样片和购买
解决方案
文件
工具与软件
质量与可靠性
eDesignSuite
开始
Partner products
Sales Briefcase

产品概述

描述

The STSW-IMG008 is a graphical user interface (GUI) for Windows 7, Windows 8, and Windows 10. The GUI controls the P-NUCLEO-53L1A1 pack which consists of the X-NUCLEO-53L1A1 expansion board connected to the STM32F401RE nucleo board. It is possible to control one VL53L1X external breakout board when it is connected to the X-NUCLEO-53L1A1 expansion board through one of the dedicated connectors.
The VL53L1X is the latest product based on ST’s patented FlightSenseTM technology. This is a ground-breaking technology allowing absolute long-distance to be measured independently of the target reflectance. Instead of estimating the distance by measuring the amount of light reflected back from the object (which is significantly influenced by color and surface), the VL53L1X precisely measures the time the light takes to travel to the nearest object and reflect back to the sensor (Time-of-Flight).
To install the STSW-IMG008 GUI, refer to the X-NUCLEO-53L1A1 quick start guide.
  • 所有功能

    • Live display of:
      • Ranging distance in centimeters
      • Signal strength
    • Region-of-interest (ROI) on the sensing array; size and position are programmable
    • Calibration procedure
    • Maximum and minimum ranging threshold controls
    • Data log outputs
    • I2C transaction recording

获取软件

特别推荐