X-CUBE-6180XA1

批量生产

STM32Cube的接近、手势、环境光传感器软件扩展

获取软件 下载数据摘要
概述
样片和购买
解决方案
文件
工具与软件
质量与可靠性
eDesignSuite
开始
Partner products
Sales Briefcase

产品概述

描述

The X-CUBE-6180XA1 software package is an expansion for STM32Cube, associated with the X-NUCLEO-6180XA1 expansion board for STM32. The source code of this package is based on STM32Cube and is aligned with the “Multi-Platform” file & directory structure to ease portability and code sharing across different STM32 MCU families.
The VL6180X is the latest product based on ST’s patented FlightSenseTMtechnology. This is a ground-breaking technology allowing absolute distance to be measured independent of target reflectance. Instead of estimating the distance by measuring the amount of light reflected back from the object (which is significantly influenced by color and surface), the VL6180X precisely measures the time the light takes to travel to the nearest object and reflect back to the sensor (Time-of-Flight).
  • 所有功能

    • Driver layer (VL6180X API) for complete management of the VL6180X proximity & ambient light sensor (ALS) integrated in theX-NUCLEO-6180XA1 expansion board.
    • Easy portability across different MCU families, thanks to STM32Cube.
    • Free, user-friendly license terms.
    • Example code for ranging and ALS measurement.
    • Example code for ranging with multiple VL6180X sensors. Up to 4x VL6180X devices can be controlled using the X-NUCLEO-6180XA1 expansion board equipped with 3x satellites (VL6180X-SATEL).
    • Example code of gesture recognition.

获取软件

您可能还会喜欢...

特别推荐

ST最新信息

All tools & software

    • 产品型号
      状态
      描述
      类型
      供应商

      X-NUCLEO-6180XA1

      批量生产

      STM32 Nucleo的接近和环境光传感器扩展板,基于VL6180X

      影像IC评估板 ST
      X-NUCLEO-6180XA1

      描述:

      STM32 Nucleo的接近和环境光传感器扩展板,基于VL6180X